The design rules check (DRC) is an elementary function of VisualApplets. A design rules check checks if a VisualApplets project does not contain any design errors. Projects which do not pass the DRC can not be build or some functions are disabled.
The DRC log window which is part of the dock, lists the progress and results of the DRCs. It shows important information on design errors and resource usage estimations. Some windows include a DRC log as a sub-window. The DRC log can be saved in a HTML file using a right click in the text and the selection of on the pop-up menu.
In VisualApplets includes two levels of design rules checks. DRC level 1 and DRC level 2 which are explained in detail in the following sections.
The DRC level 1 checks the integrity of the project. Click on Ctrl+F7 ) or use the icon Design Rules Check Level 1 from the Build icon bar to start the DRC level 1. Besides the direct access, the DRC level 1 is automatically started by other VisualApplets functions such as simulation, resource estimation, or build process. The DRC level 1 checks amongst others that
→ (- no open ports exist in a design.
- no link is in conflict state.
- no operator parameter is in conflict state.
- no conflicts for device resources exist.
The following figure shows an error reported by the DRC level 1. In this example, a device resource conflict of resource DMA is shown. You can simply click on the module name to highlight the module in the diagram which causes the error. This is very useful in complex projects with many diagram windows.
The DRC level 2 can only be started after a successful DRC level 1. However, starting the DRC level 2 by a click on Ctrl+F8 ) or a click on the icon Design Rules Check Level 2 from the Build icon bar will automatically start DRC level 1, too. Besides the direct access, the DRC level 2 is automatically started by other VisualApplets functions such as the resource estimation and build process. The DRC level 2 performs a low level design rules check and estimates the required FPGA resources.
→ (